User Activity

Hello,When using device as temperature measurement server and device joins to the network where coordinator is also trust center, joining to the network works fine, but binding not. I wander, why device don't send Active Enpoint Response message when...
Hello,I have still connection problem to Tuya gateway. Simple OnOff application can connect to Tuya gateway, but when I try to connect STM32WB5MM-DK as a temperature sensor, connection fails.Connection to Tuya gateway succeeds with STM32WB5MM-DK exam...
Hello,I have STM32WB5MM-DK evaluation kit and I am trying to get example Zigbee_OnOff_Client_Router working. I updated FUS (v. 1.2.0) and Zigbee FFD (v.1.18.0). Example do not work, I get an error "Fatal Error" on terminal and display:[M4 APPLICATION...
Hello,How should I make connection to the Tuya gateway with zigbee? I have read zigbee wiki dokumentation about zigbee binding. I have understand that I should use "find and bind" mechanism in that case. I tried to find suitable example from github, ...
Kudos from