User Activity

Hi,It's already really frustrating & time consuming to get help from ST.They ask you to create support tickets.They say we can't help you if you are not specific.To be more specific, I tried adding comments to the already created ticket and I keep ge...
Hi,I have the following board : NUCLEO-F429ZIThe datasheet says that UART3 is the STLINK UART that can be used over USB.I configured this UART but when I try to receive anything from the terminal that is connected to the UART com port, I don't see th...
Hi,I am trying to create a User Application where I pass in commands from a terminal application (ex: Putty or Ucon) which results in the motor doing something.I have configured the MC Workbench with the following options:   Not using the MC Pilot so...
Hi,I have done version control and CI-CD for large-scale C & C++ projects but I am not sure how to do this for the STM32-based tools and projects generated.For the Motor Control Firmware Development task I am currently assigned, I need to develop a s...
Hi,I am currently working on a project where I have to develop the firmware for the BLDC motors used in our device. I have been struggling to use this board along with the MCSDK as advertised. I want to get started by sending data over USART1 (open f...
Kudos from
Kudos given to