Posted on February 11, 2015 at 15:24
Hello,
Can someone tell me if it is possible to manage RTS/CTS signals over USB in VCP mode please ?
It seems that the CDC example can receive commands, but what should I do to set these signals in ...
Posted on October 15, 2014 at 14:52
Hello,
I would like to know if it is possible to change the value of the register FLASH_OPTCR by mapping a variable on it and to set the value in constant ? I think this is not possible because we need ...
Posted on October 15, 2014 at 16:55Sorry for my english :(I just see the ''Automatic Mode'' in st-link utility and I think it will do the job :)I will try to use the st-link utility with command line to unlock flash, program and relock the flash.Tha...
Posted on October 15, 2014 at 15:22Thanks for the response.I know about the APIs, but the purpose of my idea was to protect the flash by just flashing a software, and to not make other manipulation with other sofwtare like ''STM32 ST-LINK Utility'' ...