User Activity

Dear Community,   Once again I am struggling with CAN Filters for extended IDs using CAN2 on a STM32F765. I have the ID 0x010100 and the filter should look like 0xXX0101XX where the X hex should be ignored. One of my early approaches: uint32_t filter...
Hello community, I'm struggling to get the dual bank feature to work with the STM32F765 as in the X-CUBE-DBANK-F7 example shown. Following situation:I have two similar FWs, only a different LED is toggled. In the OB I set the nDBank to 0 and defined ...
Dear Community, even after reading what feels like 100 posts, I still can't manage to set the filter so that exclusively 2 IDs are let through.I use the extendet ID, 1 Byte IDs and have managed to let exactly one ID through with the MASK_MODE, as you...
Kudos from
Kudos given to