User Activity

Board: Custom board with STM32F105RCT6At first, I am able to Jump to internal bootloader while running the application code from SRAM and further able to connect STM programmer using UART interface. At this time the RDP flash protection was not enabl...
Board :- Custom board with STM32F105RCT6Description :- I am trying to Jump to internal bootloader when Option Byte for Read Out Protection is set to 1 (RDP Level  1).When I am jumping to internal bootloader by Disabling the Read out protection I am a...