User Activity

Hello,I'm using RFAL v2.6.0 and ST25R3911B and I get an issue with the IRQ management.Using ISO14443 Type-A tag,  the IRQ remains high causing the while loop not to exit. In this condition, the i_err bit of the main interrupt register is '1' while th...
Hi,I would like to use NXP ICODE ILT tags (ISO18000-3) with the ST25R3911B device.As ISO18000-3 is similar to ISO15693, is it possible to use stream mode (as in RFAL) to support ISO18000-3 ? Is there any HW limitation ?  If no, did any of you already...
Kudos from