Posted on September 21, 2016 at 21:29
Hi, I started to work on SPI, my intention is to read three gyroscope sensor by SPI bus,
Currently I testing SPI preipheral of my STM32 Discovery Board (STM32F407), this board has the sensor LIS302DL , w...
Posted on August 19, 2016 at 18:56
Hi everybody, I've started to use the STM32F4 Discovery, now I'm trying to use the ADC as single channel in conitnuous mode without DMA, i doesn't work , is it posible to do it?
#include ''stm32f4xx.h'...
Posted on October 01, 2014 at 19:06
Hi everybody, currently I'm working on STM32F4 discovery using Keil software, I'm implementing USART transmission at 9600 of baudrate.
I've definedUSE_STDPERIPH_DRIVER andHSE_VALUE=8000000 using the to...
Posted on September 23, 2016 at 22:35
hi barton
Thanks for your help,
Yes , i missed it, i've added it and it works, Now i can read the registers correctly, however i have noticed that the when i read the same register several times the ...
Posted on September 22, 2016 at 23:29 Hi thanks for you help, I´ve checked the PCB discovery version, and I've just realized that it was the version 2013 which use the sensor LIS3DSH , no the LIS302, Now the register are read correctly...
Posted on August 22, 2016 at 23:42Hi again clive1 with your suggestion it works fine, but i have some enquiries, when i worked with other ucontroller , when i used its ADC in continuous mode it just overwrite the new data on the old data but it does...
Posted on August 19, 2016 at 22:55 Hi again, I use UART1 to check. thanks while (1)
{ Estado = ADC_GetFlagStatus(ADC1,ADC_FLAG_EOC);
if(Estado){
ADCLect = ADC_GetConversionValue(ADC1); sprintf(texto,''ReadADC: %d Read...
Posted on August 19, 2016 at 21:52
Hi clivel1,
thanks for your answer,
I've tested with all options:
#define ADC_SampleTime_3Cycles ((uint8_t)0x00)
#define ADC_SampleTime_15Cycles ((uint8_t)0x01)
#define ADC_SampleTime_28Cycles ((...