Hi @HakanD CortexM7 devices are now supported by the new X-CUBE-DISPLAY.3.0.0 release available from both STM32CubeMX-6.7.0 and https://www.st.com/en/embedded-software/x-cube-display.htmlHowever, this new release does not support yet QuadSPI interfa...
Hi @tk.1 New HelloWorld examples from X-CUBE-DISPLAY pack are now displaying texts using the ST BSP Utilities.Please have a look to these new enhanced application from the new release of X-CUBE-DISPLAY.3.0.0 available from both STM32CubeMX-6.7.0 and...
Hi All,The X-CUBE-DISPLAY software expansion pack is providing external loaders only for the STM32CubePpogrammer tool. And only for the listed Projects of NUCLEO + X-NUCLEO-GFX combinations inside the pack.Sorry, but we're not providing external load...
Hello @dradoicic We didn't yet tested with AZRTOSH7-2.1.0 and yes there are a lot of changes included with the 2.1.0 version. Now the recommendation is to select Static Memory Allocation instead of the dynamic. That will align packs with the Native ...
Hello,Yes indeed there is a bug with 2.2.0 when using DMA.The BSP_[LCD|MEM]_WriteDataDMA was unlocking the APIs at the exit of the API call so transfers could overlaps.To continue you work until getting the new release which will provide the fix, you...