Hello,I hope you are well.I have a question about the certification of the “Programmable Bluetooth® Low Energy wireless SoC” from the “BlueNRG-LP” family: are they BQB certified?Thanks in advance
Hello, please how can I connect a STEVAL-IDB012V1 board with an arduino (if it is possible of course), if not is there a mobile application with which I can connect to this board and retrieve the pressure and acceleration values?
Hello,actually, i'm searching some reference of Bluetooth module without pairing, i want that the Bluetooth module communicate directly without paring.Can you give some references please ?Thanks
Hello,actually, i'm using the bluetooth module BlueNRG-M2 , and i want to know the communication distance in meter please and the length of the antenna .Thank you
Hello @Andrew Neil I have question please For example, if a module has an emission output power of 8 dBm but I want to use it at its maximum for 5 or 6 dBm only (to have less current consumption), to do this do I just need to modify the configuration...
I see that probably the difference is in the power delivered by the PA (power amplifier, the PA can be configurable ? means that for example if i need to use the bluetooth module for short range or long range the can i configure the PA ?Thanks