The FR_NOT_READY error typically indicates that the physical drive cannot be initialized due to no medium or a hard error. This could be due to a variety of reasons such as incorrect wiring, incorrect SDIO configuration, or an issue with the SD card ...
It seems you are trying to create a new project for the XCore407I board using the STM32CubeIDE, but you are unable to find the XCore407I in the Board Selector. This could be because the XCore407I board is not directly supported in the STM32CubeIDE. H...
Rotating widgets in TouchGFX without using the Image related widgets is not directly supported. TouchGFX is designed to work with static widgets and does not provide a built-in method for rotating non-image widgets.However, you can achieve this effec...
Based on the context provided, it seems you are looking to automate the naming of your output binary files in STM32CubeIDE based on preprocessor definitions. Unfortunately, STM32CubeIDE does not provide a built-in feature to customize the output bina...
It seems you are trying to create a new project for the XCore407I board using the STM32CubeIDE, but you are unable to find the XCore407I in the Board Selector. This could be because the XCore407I board is not directly supported in the STM32CubeIDE.Ho...