User Activity

Hi all,Since the TSC1641 is just a monitor (it doesn’t drive any current), I assume the internal temperature sensor is meant to measure the temperature of something nearby.In this application, I was thinking the shunt resistor could be placed on the ...
Hi experts,I'm adding to my existing code (that runs on a STM32F105) a function to store a word in the flash.I basically copied the code from the official example based on the HAL libraries, here my function:uint32_t FLASH_Write_Data(uint32_t StartPa...
Kudos from
Kudos given to