Hello @Aboyh
As a starting point, I suggest you refer to the BLE_p2pRouteur example for the STM32WB Nucleo board. Then you can try to connect your server nodes (ESP32 or else) to the STM32 Router. Also, you can connect this router to a BLE app on th...
Hello @FurkanYilmaz-97
Exactly, CN9 pins can be configured and use as ADC Inputs.
You can Show the Values on the Screen using some TouchGFX configurations.
Best Regards.
STTwo-32
Hello @FurkanYilmaz-97 and welcome to the ST Community .
In fact, you can use all the Pins on the Arduino CN9 connector as ADC inputs:
For the Red or yellow marks next to an interface, it will show you the pin conflicts (for example here IN2 is not...
Hello @saochandan
This note concern only the UFQFPN48 and the UFQFPN32. The UFQFPN24 package is not concerned by the exposed pad so this note is not applicable in this case.
Best Regards.
STTwo-32