Hi,In the Datasheet there is only a diagram for the ADC in single-ended mode.What is the circuit for differential mode:For instance, does it re-use the same capacitor across the two inputs or does it use two capacitors, one for each input?ThanksAlex
Hi Kaouthar,Are either of those two capacitors used for the single-ended conversion?Are they the same value as the single ended capacitor?The reason I'm asking is to get an idea of crosstalk when multiplexing between several sources, which may be a v...