User Activity

Posted on August 22, 2014 at 15:38Hello, I want my STM32F4Disco to communicate with an external ADC I2C, in reading mode, this last will send to the master 2 bytes ! The problem, and I don't know if it's one, the first byte sent by the slave MUST be...
Posted on August 20, 2014 at 10:23Hello, First of all, I want to determine how many output compare channel  the STM32F407VGT6 (STM32F4DISCO'S MCU) has. In the PIC32 MCU's for example, Output Compares are regarded as separate devices even if they nee...
Posted on August 18, 2014 at 23:20Hello,First of all, In a PIC32 environment, I usually fix a value for the heap somewhere in the IDE project settings, do I have to consider this while working with Atollic and STM32F4 ?I am new to STM32 MCU's and I ...
Posted on August 18, 2014 at 16:20Hello,I'm discovering the STM32F407 with an STM32F4Discovery, in the past, I worked with a PIC32, and I see that there is many differences between those two microcontrollers.I want to understand how the UART periphe...
Posted on July 21, 2014 at 10:24Hello,When I connect an ethernet cable to the expansion kit, the RJ45 LEDs are not lighting, it that normal ? they are lit once, but after never even disconnecting the board. that's strange !With a PIC32 starter kit w...