cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery Exapansion kit - Ethernet connector

mohamed-amine
Associate II
Posted on July 21, 2014 at 10:24

Hello,

When I connect an ethernet cable to the expansion kit, the RJ45 LEDs are not lighting, it that normal ? they are lit once, but after never even disconnecting the board. that's strange !

With a PIC32 starter kit when I plug an ethernet cable, the RJ45 LEDs are lighting and/or blinking.

I can't test an Ethernet project right now because I have other things to do.

I want to ensure that the expansion kit's ethernet PHY module is not defective.

Thanks in advance for your support.
3 REPLIES 3
Posted on July 21, 2014 at 14:57

The STM32F4-DIS-BB, or something else?

Aren't there code example that could be tested quickly?

Generally you'd need to configure (pins, clocks, mode) and drive the negotiation of the external PHY in your code implementation, and recognized cable in/out events and renegotiate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mohamed-amine
Associate II
Posted on July 22, 2014 at 12:24

yes, STM32F4-DIS-BB (from element14)

so you think it's a normal behaviour ? because as I sais, with a PIC32 ESK (microchip) when you plug an ethernet cable its LED begin to light, blink or both...

I'm new to STM32 MCUs so before playing with Ethernet, I should play with GPIO and the other peripherals, by the way, I'm using open source tools to develop with that target (Eclipse, OpenOCD, GNU ARM tools etc... it wasn't easy to fix ;) )
mohamed-amine
Associate II
Posted on July 22, 2014 at 12:33

Everything's ok !!! now the connector LED's are lighting !!!

I think because STLINK driver is installed on my computer !