baraadalaq
Associate
since
2023-09-14
2023-09-29
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About baraadalaq
Options
Report User
User Activity
Posts
Replies
LIS2DE12 - Sleep to Wake Function
2023-09-25
Hello,I'm looking to see if there is a maximum value for the sleep-to-wake interrupt register on the LIS2DE12. I do see +/- 2g, 4g, 8g, 16g as standard values, but is it okay to set a threshold value to +/-30g, 25g or 20g?Thanks!
Re: LIS2DE12 - Sleep to Wake Function
2023-09-29
Thanks for the reply. Would the device become unstable past the maximum value?