cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DE12 - Sleep to Wake Function

baraadalaq
Associate

Hello,

I'm looking to see if there is a maximum value for the sleep-to-wake interrupt register on the LIS2DE12. I do see +/- 2g, 4g, 8g, 16g as standard values, but is it okay to set a threshold value to +/-30g, 25g or 20g?

Thanks!

2 REPLIES 2
Federica Bossi
ST Employee

Hi @baraadalaq ,

Welcome to ST Community!

You need to stay within the FS range, so at maximum value of 16g.

If my reply answered your question, please click on Accept as Solution at the bottom of this post. This will help other users with the same issue to find the answer faster :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Thanks for the reply. Would the device become unstable past the maximum value?