cancel
Showing results for 
Search instead for 
Did you mean: 

SPC56EL60 Software Watchdog reset fails

Patriks
Senior
Posted on July 18, 2016 at 10:44

Hi,

I am currently using the software watchdog of SP56EL configured that the first counter time-out will raise and interrupt and the second counter time-out will reset the device. This works fine, but the controller canĀ“t be initialized correctly after the reset.It runs throught boot.sbut stops in spc_clock_init() at this part:

/* The system must be in DRUN mode on entry, if this is not the case then
it is considered a serious anomaly.*/
if (ME.GS.B.S_CURRENT_MODE != SPC5_RUNMODE_DRUN) {
SPC5_CLOCK_FAILURE_HOOK();
}

I think the reason isthat controller is still in SAFE mode and not as it should be in DRUN mode at this time. Is this a missing part of implemenation in boot.s or do i have to change anything manually? What would be the correct actions for a correct reset after software watchdog time out?

Best regards,

Patrik

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
procolo
Senior
Posted on July 19, 2016 at 12:38

procolo
Senior
Posted on July 19, 2016 at 12:39

Hi Patrick,

unless you have modified Reset Generation Module (RGM) registers, device will wake up in DRUN mode after a SWT reset.

As reported in Reference Manual when a functional reset occurs (SWT is a functional reset in Leopard platform):

 ''During this entire process, the MC_ME state machine is held in RESET mode. Only at the end of the reset sequence, when

the IDLE phase is reached, does the MC_ME enter the DRUN mode''

So, I would suggest two possible explanations/corrections to your problem:

1) the RGM module (which performs a reset in 4 steps) as not yet gone in IDLE mode and so DRUN mode is not yet active

when spc5clockinit function check the current mode. In this case you can put a while loop before DRUN mode check ,

waiting for device to be ready

2) for some reason we'll investigate, device is really in SAFE mode. in this case first check if device is really in

safe mode, than can force DRUN mode by issuing  SPCSetRunMode(SPC5_RUNMODE_DRUN).

Feel free to contact me for any other questions.

Regards,

Procolo