Hello
ESDALY is a good choice. Since the operating voltage is 5V, ESDA6V1LY should be used, as Vrm = 5.25V (for ESDA5V3LY, Vrm = 3V).
If you have more than 2 lines to protect that are close to each other, you can also use:
ESDA6V1-5SC6Y, 5 lines, aut...
Hello Mario,
Pads circled in yellow are connected to GND. However, no need to connect them to GND.
CAD files have been modified to be in accordance with datasheet footprint recommandation.
Best regards.
Fabrice.
Hello,
For TMDS/FRL lines, I recommend to use ECMF4-40A100N10, or ECMF4-2450A60N10.
ECMF4-2450A17M10 is on NRND status.
Solutions to protect and filter HDMI connector signal are presented on AN5121.
Regards.
Fabrice.
Hello,
ECMF4-40A100N10 can be used for protecting USB3.2 Gen2x2 Superspeed TX and RX lines.
Eye diagram measurements have been performed for 5Gbps and 10Gbps, according to test setup defined in USB 3.2 standard (i.e. reference cable, equalizer and D...