User Activity

Hi,I am using built-in usart bootloader on stm32g0. And I am also using the same usart for communication in my user app. I enabled the bootloader via boot option bits. When I start the debug session, I can see the flow stepping over through the progr...
We developed custom PCB with CR95HF on it. PCB on itself was tested and RF circuit tuned(PCB and antenna design is based on development kit), antenna frequency is at 13.56MHz(+/- 0.5KHz), at around -60dB, uart communication working, can put CR95HF to...
Hi, we are studying option of upgrading one of our existing projects that already incorporates the VL53L5 sensor with the STs EdgeAI machine learning library, that would enable our product to use data from the ToF sensor to learn patterns and detect ...