SofLit has a decent link to some documentation, and it's also in the Nucleo-144 MB1363 (UM2408) section 6.4.8 to show what solder pads to use. My software-only solution came from observing that booting up at lower clock rates and then switching to 48...
I'm guessing either you didn't read and/or understand my posting. Without changing solder pad jumpers, when I set LDO/VS0, it works until power down/power up, at which point it locks up (race condition). By booting up and setting SMPS FIRST, and THE...
I know this is an old thread, thought I'd add a helpful tidbit. I had the darndest time getting the board to work at 480MHz, and when I got it (LDO, VC0) the board locked up when powering on. Once it was properly booted with a 240MHz build, I could f...