The Nucleo also works on MacOS. Please read the chapter B5.2.2 of ARM IHI 0031E, you must send the value 0x79E7 (MSB first) somewhere in your init sequence. The sequence you describe is wrong, if your description is exhaustive.
Hello,I don't see in your description the "Switching from JTAG to SWD operation" sequence described in chapter B5.2.2 of ARM IHI 0031E, required after target power on and between the reset and idle sequences. The STM32L053 does not implement the dorm...
Hello,my understanding is that you are attempting to develop your own host SWD interface/debugger in place of existing solutions, is that right ? It is a relatively ambitious objective for which it will be difficult for us to provide support. The SWD...
Hello,The ST-Link firmware is expected to automatically activate the 5V output when conditions are met for that; typically, in case no signal is present on pin22 at ST-Link startup, when the USB enumeration is completed by the host. This is because t...
Hello,Initially boards have been produced with a single MCO output value: 8MHz, generated from the internal HSI of the STM32F723. Afterwards, several versions of ST-Link firmware have been published to extend this behavior; the last modification is a...