Here,PF2_NRST pin (Pin Number - 4) is configured as digital input pin.And PA13 pin (Pin Number- 7) is configured as digital output.When toggling the pin PA13, getting proper voltage level 3.3 volts and 0 volt. While reading low level on the input pin...