User Activity

Hello,I want to read which stack is updated in my controller. For example stm32wb5x_BLE_Stack_full_extended_fw / stm32wb5x_BLE_Stack_light_fw / stm32wb5x_BLE_Zigbee_RFD_static_fw. So can I read back the stack name using code? Is there any way to read...
Hello,I ordered this IC for one of my products and am confused about the SPI modes. In the datasheet, it is mentioned that it will support SPI mode 0 and mode 3, but I have not found any timing diagram of SPI mode 0 in the datasheet. Can you provide ...
Hi there,I was working on the LIS2DH12 for one of our applications and found that the LSI2DH12 is not able to work on a supply voltage greater than 2.7V. Is there any condition to operate the device on a voltage greater than 2.7V? In my application, ...
Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...
Hello,I am using LIS2DH12TR through SPI but I am not able to operate it on greater than 2.8V. On greater than 2.8V I am not able to read the device ID. But according to the datasheet, it is able to operate up to 3.6 V. SO how can I use this ic greate...