If you count the answers and the replies you got, I think that you will known whats is going on with this software package.If you define USE_USBD_COMPOSITE you will encounter a lot of errors.Not just bugs but great ERRORS.
Had the same problem.I only have a speaker no microphone.Mine solution:In USBD_AUDIO_IsoINIncomplete():I do not check if the feedback endpoint is the cause of the INIncomplete interrupt.I do not flush that endpoint (but you can do).But I always DO (M...
Yes, same problem here.Lcd 320*240 pixels and 2 bytes/pixel.This is a total of 320*240*2 = 150kB.TouchGFX 4.17:Partial buffer strategy.3 blocks.40kB/block.On init (total area of LCD is invalid) TouchGFX could update the LCD in 150/40 is 4 steps.But T...