cancel
Showing results for 
Search instead for 
Did you mean: 

Are TouchCalibration calculation incorrect? Why is there an offset in the calcutated values?

IPiSw.1
Associate II

TouchCalibration tsCalibration;  // TouchGFX 4.17

MATRIX matrix ;           // Carlos E. Vidales

touchgfx::Point lcdCalibPoints[3] = {

 {    0,    0},

 {    0, 240 - 1},

 {320 - 1, 240 - 1}

};

touchgfx::Point tsCalibPoints[3] = {

 {    0,    0},

 {    0, 240 - 1},

 {320 - 1, 240 - 1}

};

void STM32TouchController::init() {

  tsCalibration.setCalibrationMatrix(lcdCalibPoints, tsCalibPoints);

 setCalibrationMatrix((POINT *)lcdCalibPoints, (POINT *)tsCalibPoints, &matrix );

}

bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y) {

 POINT  display, screen ;

 touchgfx::Point tsPos;

 x = tsCalibPoints[0].x;

 y = tsCalibPoints[0].y;

 tsPos.x = x;

 tsPos.y = y;

 screen.x = x;

 screen.y = y;

 tsCalibration.translatePoint(tsPos);

 getDisplayPoint(&display, &screen, &matrix);

 // Here tsPos.x == -1,  tsPos.y == -2.   x and y should be 0 ??

 //   display.x == 0, display.y == 0

 x = tsCalibPoints[2].x;

 y = tsCalibPoints[2].y;

 tsPos.x = x;

 tsPos.y = y;

 screen.x = x;

 screen.y = y;

 tsCalibration.translatePoint(tsPos);

 getDisplayPoint(&display, &screen, &matrix);

 // Here tsPos.x == 318, tsPos.y == 237.   x should be 319 and y should be 239 ??

 //   display.x == 319, display.y == 239

  

 return false;

}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
IPiSw.1
Associate II

Additional info:

tsCalibration.matrix.An == matrix.An

tsCalibration.matrix.Bn == matrix.Bn

tsCalibration.matrix.Cn == matrix.Cn

tsCalibration.matrix.Dn == matrix.Dn

tsCalibration.matrix.En == matrix.En

tsCalibration.matrix.Fn == matrix.Fn

tsCalibration.matrix.Divider == matrix.Divider

tsCalibration.matrix.clzuAn no such field in matrix

tsCalibration.matrix.clzuBn no such field in matrix

tsCalibration.matrix.clzuDn no such field in matrix

tsCalibration.matrix.clzuEn no such field in matrix