Hello,I notice in the STM32G030x6/x8 datasheet, Table 18 that the max input voltage on FT_xx and any other pin are VDD + 4V and 4V respectively. Does this mean those pins can be safely driven with 3.3V when the MCU is unpowered?Thanks,Nicholas
Hello, I have 2 clarification questions on the default VDDSMPS configuration for the STM32H745:I notice multiple times in the STM32H745xI/G datasheet that "VDDSMPS must be kept the same voltage level as VDD." Similarly, RM0399 also has a note that VD...