Hi,I have a custom board with an STM32H745 which doesn't boot / I can't connect to.I've noticed that three of the gnd pins are not connected K15, L15, M15, would this cause the problem?The design is using an external 1.2V supply which is fine. 3.3V i...