cancel
Showing results for 
Search instead for 
Did you mean: 

reason H745 not booting

SHanl.1
Associate

Hi,

I have a custom board with an STM32H745 which doesn't boot / I can't connect to.

I've noticed that three of the gnd pins are not connected K15, L15, M15, would this cause the problem?

The design is using an external 1.2V supply which is fine. 3.3V is also fine.

I'm seeing 1.2V on the reset pin.

Any thoughts?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

Unconnected power pins may caus all kind of headaches. Fix that. Check also power sequencing requirements.

TDK
Super User

All power pins are required. The chip will not run without them connected.

If you feel a post has answered your question, please click "Accept as Solution".