@DCook.1I figured the issue I had. You need to make sure that the memory paging is set up correctly and the FLASH_DESC_STR is set correctly in usbd_dfu_if.c. In my case I am using the STM32L4P5CGTxP, so I set it to the following: #define FLASH_DESC_S...
Hello,I am also getting a Hard Reset that is set in the UCPD SR (status register) (Rx Hard Reset detect interrupt), every single time during power negotation after the Source sends accept, and Sink sends a Good CRC. Hard Reset is seen, and stops the ...