User Activity

I have been able to compile and load the X-CUBE-SPN5 example to my NUCLEO-F401 with an IHM05A1 board. I notice in the example folders that there is a BSP folder with L6208 component and MotorControl folders. How can I make these folders/drivers acces...
I have downloaded and installed the SPINFamily setup msi file. The User Manual UM2022 page A.3 describes programming the nucleo board with the firmware file guifw-STM32XXXXX-nucleo.binI have not been able to locate this file for the F401RE Nucleo boa...
I have downloaded a copy of the en.x-cube-spn5 but I am unsure how to add this to the STM32CUBEIDE to allow me to run the example programs. I would then like to develop new applications using a pair of X-NUCLEO-IHM05A1 boards and a Nucleo-F401RE boar...