Thanks markof, I got it to work. I followed your steps and once I got the 64-bit version of MX, I was successful at creating the .project. Strangely, I had to try a couple of times until it worked. Now that I have the IDE project setup, when I updat...
I will try this. Should I also uninstall and reinstall CubeIDE or just CubeMX? Maybe the issue was that I installed CubeMX before I installed CubeIDE originally?
Only a .mxproject and .ioc file is created. I don't see any .project or .cproject. If I use the IDE to create the .ioc, I am unable to point the project to the correct firmware location, so I can't win in that direction either.
Hello. I've installed the latest CubeMX and CubeIDE versions, 5.5.0 and 1.2.0 respectively and I have the same issue. If I use MX to generate a CubeIDE project, it says the same error message as indicated in other posts above, "Toolchain Settings: P...