>I said 10k and that's what ST recommends.After replacing the 100k with 10k it still does not work.>I thought you have connected it to the debugger's RST pin!?Yes indeed I did, but I also got a switch, I did this for the certainty that it works.
@Piranha A type fault of me , I mean I put two 12 pF capacitors, and yes that right it has to start with the internal oscillator anyway. Yes I have put an 100k resistor from BOOT0 to GND and disconnected 47k pull-up resistor from NRST but it still do...
The first signs-of-life methode1 : Pin 1 is marked here, is this right? The datasheet was bit confusing but this seems right to me? This seems to be right, I connected the 3.3V and GND as shown in the picture, also the SWDIO and SWCLK and reset pin. ...