User Activity

Hello all,I am trying out different projects based on the F469I discovery board. Unfortunately they show up in STM32CubeIDE as having the same name, so it refused to open them.This problem has been around for a long time, with a rather ugly workaroun...
Hello all,I have used TouchGFX for one project before (see https://www.eevblog.com/forum/projects/high-voltage-electronic-load-(500v-500ma)/msg4833872/#msg4833872)which was lots of trial and error, following some tutorials. I still find the architect...
Hello all,I'll be starting a project in TouchGFX designer from an existing template, say STM32F469I DISCO. How does the code generation by the TouchGFX designer and CubeMX interact? Say when I add an UI element and regenerate the code in designer, do...
Hi all,I have a STM32G474 and data in backup registers (eg. LL_RTC_BKP_DR0) are cleared after reset or power cycle (3.3 V battery is present!).Code is generated by CubeMX with LL drivers. I enabled RTC and disabled all tampers.In the main code, I can...
On the STDC connector, Pin 13/14 are virtual com port signals T_VCP_RX and _TX.Which one is input and output? They have cryptic comments like "Output for STLINK-V3SET" (for _RX) - Is RX an output and connects to the RX pin on the STM32? Or is it an i...
Kudos from
Kudos given to