I just updated TouchGFX designer from version 4.2.0 to 4.21.0. Trying to open my projects saved last time with version 4.2.0, I'm obliged to update them to the new version. After this, they are all corrupted.
Question 1:We are developing a custom board based on STM32H750B-DK.We have a “custom touch�? on it, so I have to adapt the “component�? to CubeMX-TouchGFX structure.The question: in the STM32H750B-DK project template we find files stm32h750b_discover...
Hi Osnam,I updated the image names as you suggested, and stored the project with TouchGFX 4.20.Then I reopened it with TouchGFX 4.21.1, and finally everything worked fine!Thank you very much for support!
here attached 2 screenshots. When I try to open a project, I receive the message I need to convert it (screenshot 1); if I say "no", it doesn't open. If I say "yes", the error (input string was not in correct format) appears in very short time (few s...