User Activity

Hello,my project expands and i need more than 32k flash.In the CubeMX it is not possible to change the Mcu Referenc.It is possible without to generate the project new to change the Mcu?Thanks
Posted on September 01, 2015 at 18:36Hello, i use EEPROM simulation and sometime i must use the flash page erase for new data. If during the erase time there is one ore more pending ISR, the system crashed. After reboot with the watchdog i found, th...
Posted on February 02, 2014 at 10:50Hello, my input capture code TIM1_CH3 (PA10) works very well on an F100 or F103, but not on the STM32F051. If i submit the debug session of the test code the GPIO and TIM1 register looks like ok. It looks like an ...