Trying to compile (cube ide 1.11.0) the generated code from the attached ioc (which is the first example of the BLE mesh MOOC) generates a long list of "undefined references"I had to reverse to MX 6.6 and WB 1.14.1 and works just fine
Hi Semer, the steps are stated in the first post, including the SW and versions used. Can't provide the console output given that I had to roll back in order to be able to keep working.If st wants to reproduce the error, is as easy as to download th...
When you generate code from cubemx and try to compile it without any modifications, you should not have linker or whatsoever errors.And as stated, this works fine with the previous version of MX and WB...