I am using ADC regular simultaneous mode with stm32f427It works nice with the pulse signal is comming after dma start(HAL_ADCEx_MultiModeStart_DMA)but if the signal is comming before calling ADC dma start code it going to infinityhow to solve this?i ...
I've used triple regular simultaneous mode only before(stm32f427zgt6)but now i try this with updated cube mx version, i cannot find itIs it deleted? so now i am trying combined regular simultaneious but it is no
My board is now on brickI dont know why this happen but i want operate system boot loaderBut i can not find that pin on my board where can i find that resister?
Hi i'm trying tcp server with stm32f427 which combined LAN8720A phy chipI got a problem with this codeHAL_StatusTypeDef HAL_ETH_Init(ETH_HandleTypeDef *heth)
{
uint32_t tickstart;
if (heth == NULL)
{
return HAL_ERROR;
}
if (heth->gSta...
Data sheet seems like saying "DAC_O UT min(2) Lower DAC_OUT voltage with buffer ON's value is higher than 0.2[V]"So there's nothing we can do with only using code..?I captured the parts of pointing DAC out minimum