User Activity

I have a new product using the stm32l486, and the GPIOG pins mentioned in the title do not appear to work as outputs, even though they are configured identically to the GPIO pins I am using for ports A-F. I cannot find anything in either the datashe...
I am using the ST32CubeIDE and the imported HeartRate project from the STM32CubeWB package. For both boards the project compiles and is loaded into the board, and then the boards just stop working during debugging. I am not probing the boards or t...