HelloJust change line 119 of main activity the PendingIntent.FLAG_IMMUTABLEtoPendingIntent.FLAG_MUTABLEand you will discover Tags.Concerning the class TagDiscovery.java, it is updates according to our released Tags.Hope this help?BR, FB
HelloThaks for the feedback.I did some tests on several phones with different Android versions (Pixel3/Android12, Pixel 6Pro/Android14) without reproducing the issue.The NFCTap version is (menu/About) : V3.10.0 with ST25SDK:1.10.0 (The last posted on...
I see that you use @ mode, i suggest that you use 0x22 for FlagsFor information:In addressed mode (i.e. with UID parameter in the request), the Address_flag (bit 6) shall be set to 1. Usually Data_rate_flag (b2) is also set to 1 (High data rate shall...
HelloI see that you use @ mode, i suggest that you use 0x22 for FlagsFor information:In addressed mode (i.e. with UID parameter in the request), the Address_flag (bit 6) shall be set to 1. Usually Data_rate_flag (b2) is also set to 1 (High data rate ...
HelloSorry, but the answer is no, because in most of cases you have to synchronize, app and ST25DV to exchange data ... You can rely on Mailbox Management activity (Android sources available on ST web site) to get basis for a simple approach.BR, FB