User Activity

Is it correct that the WirelessFwInfo_t.MemorySizeSram2A/B members describe the wireless stack occupied areas of SRAM2 in terms of 1k units (growing downwards)?I am noticing there is memory being written to at 0x20031000 onwards, but that doesn't lin...
I cannot get the Phy_802_15_4_Cli example project working on our custom board (as part of certification). Seems like there is something wrong with the CM0 / CPU2 core, but I have no idea what the return codes mean.Only things I have changed in the ex...
Some strange behavior is happening when debugging our firmware through STM32CubeIDE, where it erases the option bytes upon flashing the firmware (0xFF @ 0x1FFF8000 onwards). The debugging session still launches ok and the firmware appears to be flash...
Kudos from