Nuser
Associate II
since
2019-10-24
2023-06-14
User statistics
9
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About Nuser
Options
Report User
User Activity
Posts
Replies
Nucleo-L432KC : Generated Code Will Not Compile ADC_CHANNEL_DAC1CH2_ADC2
2019-10-24
Requesting "VDAC1_OUT2 Channel" on ADC IN18 causes the .ioc file to generate the following line:- sConfig.Channel = ADC_CHANNEL_DAC1CH2_ADC2;which doesn't compile, I think it should be:- sConfig.Channel = ADC_CHANNEL_DAC1CH2;
Re: Nucleo-L432KC : Generated Code Will Not Compile ADC_CHANNEL_DAC1CH2_ADC2
2021-03-01
Of course, it is attached.
Re: Nucleo-L432KC : Generated Code Will Not Compile ADC_CHANNEL_DAC1CH2_ADC2
2021-03-01
This issue is still not fixed as 01-MAR-2021. IDE V 1.6.0 and FW Package STM32L4 1.17.0There is no ADC2 in the chip!