User Activity

Hello,I have an interesting situation. When I start my app on the F303RE Nucleo I initialize all the peripherals. When CAN is initialized it returns a HAL_TIMEOUT error. If I call the same initialization code a second time it initialized correctly...
Hello. I have a project that runs fine on F303RE Nucleo board. I loaded it on the F303ZE Nucleo board and I get no banner displayed on the Virtual Comm port. The device manager sees the port fine. Are there any solder bridges or jumpers needed...
Hello,I have a project working on the F303-re Nucleo board. I want to run it now on the F303-ze Nucleo board. Apparently virtual com port doesn't work the same on the ZE as it does on the RE. I can take a new RE board, copy the binary file to th...
Kudos from