User Activity

Hi,I need to periodically count the number of pulses of signal A between two rising edges of signal B. For that I use a timer (TIM2) in ETR mode (signal A is the ETR input), input capture on signal B and slave trigger+reset on signal B rising edge.No...
Hello,I need to count the number of (positive and negative) edges in a signal within certain time period. For that I use a timer on STM32L452. The AN4776 says that External Clock Mode 1 is able to update the counter on both edges (for the price of no...