when i don't blow but when i breathe, i.e. warm air, the value changes.As I have already described before that the pressure only changes when I put my finger on it and the sensor assimilates my body temperature.the device does not hang because the te...
Hi @Eleon BORLINI My conversion is correct. Even if I didn't have the conversion right, the value would at least have to move in some direction, but it doesn't. The value that my software outputs is identical to that of the Unico GUI in connection w...
oh yes I forgot to mention that the 78mbar are relative.I have two of the sensors.Which also amazes me that the two sensors will display different ones when idling.one sensor shows 1021 hPa absolute when idling and the second sensor 996 hPa.I don't u...
To confirm that my application is tight, I installed the board with the sensor in a separate housing.Unfortunately, the value does not change in the Unico GUI.The GREISINGER measuring device shows a negative pressure of approx. 78 mbar in the housing...