User Activity

Hi,I just downloaded the latest cryptolib v4 and read in the docs that it is not compatible with v3 anymore.Are there any instructions how to use it with the "STM32 Security in practice" workshop?Thanks,Anguel
Projects do not build when one tries to use the new headless build syntax from the 1.7 manual.Manually extracting headless-build.bat from the 1.7 installer and copying over to the STM32CubeIDE directory solves the problem.
Hi,Let's say I have a workspace with multiple projects (e.g. application project, bootloader project, etc.) for a product. Let's say this workspace is located in C:\ProductA. Now I would like to duplicate this workspace to use it for another product ...
An error occurred while collecting items to be installedsession context was:(profile=STM32CubeIDE, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).No repository found containing: osgi.bundle,com.st.stm32cube.common.mx,...
Hi,I am developing a bootloader and an application for a device. Now I have two separate projects and I configure all pins using CubeMX twice. Each project has ist own .ioc file and it is very much work to synch all pins and other settings between th...
Kudos from