User Activity

While doing heavy activity with a NAND flash, the code is generally working, but occasionally I get hung up waiting for an operation to finish. I trapped it on the logic analyzer several times, and it's never at the same time. In every instance the ...
Some setting in the .ioc file causes it to put many links into the project for files that are already in the source tree. This results in hundreds for duplicate symbols. They are in several directories How can I stop it from doing that?
I'm using libraries from outside the project tree so I need to define symbols and add include directories. But every time I regenerate code with CubeMX, my additions are overwritten. Is there any place or method I can add to those options that won't...
I have WB55 Dongle board that someone may have programmed previously. I am trying to start it fresh and make sure it is up to date using all files from  from STM32Cube_FW_WB_V1.2.0I followed the procedure to install new FUS and BLE Stack:STM32_Progr...
I read that STM32WB current models do not currently support a Bluetooth 5 coded PHY. Is it possible it will someday with an upgrade to the CoProc Binaries, or is it not in the silicon at all?If not does ST have any parts on the roadmap that will?