2019-09-12 5:50 AM
Hello there :)
I'm trying to use a KSZ8863 Ethernet PHY with the STM32F767. I'm using the Nucleo F767ZI Board where i unsoldered the jumpers to the onbord PHY. The KSZ8863 is then connected via the Morpho connectors.
I just used the Code generated by the CubeIDE with rtos and lwip.
By now I can configure the PHY via MIIM (MDIO, MDC) with no issue.
but I have no communikation with the Ethernet.
Looking at the RMII interface via logic-analyzer i can see the 50MHz clock. And the data send from the Phy to the STM32 with corresponding frequency.
But when i look at the Date send from the STM32 to the Phy it looks like the µC sends with a to low frequency. (if im right with 2.5MHz) . So it looks like the STM32 uses a wrong clock.
So far the only thing I could find is that
SYSCFG->PMC |= (SYSCFG_PMC_MII_RMII_SEL);
selects the used interface (and with that the clock?).
(See STM32F767 datasheet page 1776 / 42.4.4)
In the Figure 549 Clock Scheme, there is the Sync. divider. bit i cant find anything more about that.
So what am I missing? I'm stuck..
Some help would be very nice :)
Cheers
Solved! Go to Solution.
2019-09-12 6:31 AM
ok
as usual, shortly after asking around I found the issue :)
The HAL Driver does not detect the speed of the PHY and therefore uses 10M.
So to solve that in the stm32f7xx_hal_eth.c in line 443 change to 100M
because the KSZ8863 is a switch and always needs 100M at the RMII to work, one can replace the speed selection in Line 440:
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if((phyreg & PHY_SPEED_STATUS) == PHY_SPEED_STATUS)
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
else
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}with simply
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;So my question is answerd and maybe it will help others solving it :)
Cheers
2019-09-12 6:31 AM
ok
as usual, shortly after asking around I found the issue :)
The HAL Driver does not detect the speed of the PHY and therefore uses 10M.
So to solve that in the stm32f7xx_hal_eth.c in line 443 change to 100M
because the KSZ8863 is a switch and always needs 100M at the RMII to work, one can replace the speed selection in Line 440:
/* Configure the MAC with the speed fixed by the auto-negotiation process */
if((phyreg & PHY_SPEED_STATUS) == PHY_SPEED_STATUS)
{
/* Set Ethernet speed to 10M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}
else
{
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;
}with simply
/* Set Ethernet speed to 100M following the auto-negotiation */
(heth->Init).Speed = ETH_SPEED_100M;So my question is answerd and maybe it will help others solving it :)
Cheers
2025-01-14 5:18 PM
KSZ8863 has two PHYs, but when I initialize Eternet, do I have to enter the setting value as MDIO in the PHY register for both?
We are currently working on the project with Stm32f207VET6 and KSZ8863, and we have enabled Full-Duplex, Auto-Nego, and 100BaseTX with hardware pin strapping, which can communicate on both sides of the RJ45 Port, but not on the STM32 side through the port from outside.