User Activity

Is it possible to implement device HUB?(i want my f103 to appear as usb HUB to host PC)Like a compound device. Cant find any example for some reason.
Im on that new CubeIDE, all updated. My MCU is f103.Making hid device, which should have a few reports, more than 1. So, i edited report descriptor, added reportID, added second report. Windows recognizes it just fine.But what a surprise, second repo...
I have a few MCUs but do not have good dev board, if i solder STM32F373V8T6 on STM32F3discovery  board will it work?
Im using stm32f103RB on nucleo64 board, to read SPI sensor with half duplex SPI master mode.SPI blocking recive function do not disable SPI properly, it should disable it and then finish recive one more time, as user manual RM0008 specify(25.3.8), bu...
Kudos from