cancel
Showing results for 
Search instead for 
Did you mean: 

DSI Clock Frequency

DPfei.16
Associate III

Hello,

i have 25 MHz HSE Clock.

The DSI PLL settings are as follows: IDF 5, NDIV 80, ODF2

With these settings i measure an DSI clock of 100 MHz on the DSI_CKP pin.

But Cube says that the DSI clock is 200 MHz.

I use a STM32F769NI device with 2 DSI data lanes.

Do you have any idea?

BR

Daniel

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5

They do on the surface look like appropriate numbers for a 200 MHz pixel clock.

As I recall the DSI clocks on both edges, effectively doubling the bandwidth, ie 100 MHz clock on pin equates to 200 Mbps on the wire.

I built a decoder for the LTDC/DSI clocks, will have to dig that up.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DPfei.16
Associate III

Hi Clive,

thank you for your response!

I know DSI uses double data rate (DDR) and therefore data is transfered on the rising and the falling clock edge. This means when I have a DSI clock frequency of 200 MHz I have a bandwitdth of 400 Mbit/sec.

But I don't understand why the measured DSI clock frequency is only the half of the calculated DSI clock frequency.

The STM32's unit clocks at 200 MHz internally so it can generate data on both edges of the 100 MHz clock on the wire.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
void plldecode(void) // sourcer32@gmail.com
{
  uint32_t vcoinput, vco;
  uint32_t oscsource;
  uint32_t pllcfgr = RCC->PLLCFGR;
  uint32_t plli2scfgr = RCC->PLLI2SCFGR;
  uint32_t pllsaicfgr = RCC->PLLSAICFGR;
  uint32_t pllp, pllq, pllr;
  uint32_t p, q, r;
 
  /* Configure the PLLSAI division factor */
  /* PLLSAI_VCO Input  = PLL_SOURCE/PLLM */
  if((pllcfgr & RCC_PLLCFGR_PLLSRC) == RCC_PLLSOURCE_HSI)
    oscsource = HSI_VALUE; /* In Case the PLL Source is HSI (Internal Clock) */
  else
    oscsource = HSE_VALUE; /* In Case the PLL Source is HSE (External Clock) */
 
  vcoinput = (oscsource / (uint32_t)(pllcfgr & RCC_PLLCFGR_PLLM));
 
 
  vco = (vcoinput * ((pllcfgr & RCC_PLLCFGR_PLLN) >> 6));
 
  pllp = (((pllcfgr & RCC_PLLCFGR_PLLP) >> 16) + 1) * 2;
  if (pllp) p = vco / pllp; else p = 0;
 
  pllq = (pllcfgr & RCC_PLLCFGR_PLLQ) >> 24;
  if (pllq) q = vco / pllq; else q = 0;
 
  pllr = (pllcfgr & RCC_PLLCFGR_PLLR) >> 28;
  if (pllr) r = vco / pllr; else r = 0;
 
  printf("PLL    P:%9d Q:%9d R:%9d\n", p, q, r);
 
 
  vco = (vcoinput * ((plli2scfgr & RCC_PLLI2SCFGR_PLLI2SN) >> 6));
 
  pllp = (((plli2scfgr & RCC_PLLI2SCFGR_PLLI2SP) >> 16) + 1) * 2;
  if (pllp) p = vco / pllp; else p = 0;
 
  pllq = (plli2scfgr & RCC_PLLI2SCFGR_PLLI2SQ) >> 24;
  if (pllq) q = vco / pllq; else q = 0;
 
  pllr = (plli2scfgr & RCC_PLLI2SCFGR_PLLI2SR) >> 28;
  if (pllr) r = vco / pllr; else r = 0;
 
  printf("PLLI2S P:%9d Q:%9d R:%9d\n", p, q, r);
 
 
  vco = (vcoinput * ((pllsaicfgr & RCC_PLLSAICFGR_PLLSAIN) >> 6));
 
  pllp = (((pllsaicfgr & RCC_PLLSAICFGR_PLLSAIP) >> 16) + 1) * 2;
  if (pllp) p = vco / pllp; else p = 0;
 
  pllq = (pllsaicfgr & RCC_PLLSAICFGR_PLLSAIQ) >> 24; // 2..15
  if (pllq) q = vco / pllq; else q = 0;
 
  pllr = (pllsaicfgr & RCC_PLLSAICFGR_PLLSAIR) >> 28; // 2..7
  if (pllr) r = vco / pllr; else r = 0;
 
  printf("PLLSAI P:%9d Q:%9d R:%9d\n", p, q, r);
 
  {
    uint32_t dckcfgr1 = RCC->DCKCFGR1;
    uint32_t divr = 2 << ((dckcfgr1 & RCC_DCKCFGR1_PLLSAIDIVR) >> 16); // 2,4,8,16
    uint32_t lcdclk = r / divr;
    printf("LCDCLK   %9d, %6.2lf MHz\n", lcdclk, (double)lcdclk*1e-6);
  }
 
  {
    uint32_t dsiwrpcr = DSI->WRPCR;
    if (dsiwrpcr & 1) // Enabled
    {
      uint32_t odf = 1 << ((dsiwrpcr >> 16) & 0x0F); // 1,2,4,8
      uint32_t idf = ((dsiwrpcr >> 11) & 0x07);
      uint32_t ndir = ((dsiwrpcr >> 2) & 0x7F); // 10..124
      uint32_t dsi = (HSE_VALUE * ndir) / (idf * odf);
      printf("DSIPLL   %9d, %6.2lf MHz\n", dsi, (double)dsi*1e-6);
      printf("lbClk    %9.3lf KHz\n", (double)dsi / 8000.0);
      printf("TXEscape %lf\n", (double)dsi / (8000.0 * 15620.0));
    }
  }
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DPfei.16
Associate III

Hi Clive,

many thanks for your help!

BR

Daniel